Agency Listings

Silent Knight products are designed and manufactured to meet or exceed various product safety and certification requirements. To view our listings, please visit one of the following sites.

In order to make sure we provide everyone with the most up-to-date CSFM listing documents we would like to direct you to the ca.gov website.

Search Suggestions: On their site, there are three drop downs: Category, Company, and Listing.

We would suggest that you ignore the first drop down menu, "Category". In the second drop down, "Company," select 0559 -- SILENT KNIGHT SECURITY. Ignore the third drop down and just click the "Search" button. 

After the results are displayed, press Ctrl + F and then type in the Silent Knight model number you're searching for. This should take you right to the product listing of interest.

​​​​​​​​​

Factory Mutual (FM)

Visit Factory Mutual's Web-based Approval Guide (registration required) which contains up-to-date information about FM-Approved and tested products. It also includes essential engineering data and technical information on the application and use of listed products.

Includes scanned MEA listings. For more information about MEA listings, visit the New York City Department of Buildings web site.​​​​

UL is the leading Standards Development Organization for product standards and is responsible for developing and maintaining these standards under the American National Standards Institute’s (ANSI) balanced processes. A Standards Technical Panel is responsible for the development of the technical requirements and the product standards are then used by test and certification agencies known as Nationally Recognized Test Laboratories (NRTL) to test and certify products for compliance.

Many of our UL product certifications can be found here but we recommend visiting the UL Product iQ directory for the most current and complete list of UL product certifications.

Documents (23)  
FSYE.S3511 - Emergency Alarm System Accessories 
FSZI.S2766 - Emergency Alarm System Control Units 
FTAM.S6173 - Gas and Vapor Detectors and Sensors 
IP Communicator UL Listing Explanations 
IPGSM-4G UL Certificate of Compliance 
PGWM.S2766 - Control and Communication Equipment 
PGWM.S3511 - Control and Communication Equipment 
QVAX.S2766 - Process Management Equipment 
QVAX.S3511 - Process Management Equipment 
SYZV.S2766 - Control Units, Releasing Device 
UOJZ.S2766 - Control Units, System 
UOXX.S3511 - Control Unit Accessories, System 
SYSW.S3511 - Accessories, Releasing Device 
UTGT.S6173 Single- and Multiple-Station Smoke Alarms 
UNIU.S6012 - Boxes, Noncoded 
UOJZ.S24048 - Control Units, System 
UOQY.S2766 - Emergency Communication and Relocation Equipment 
UOXX.S789 - Control Unit Accessories, System 
UQGS.S6173 - Heat-automatic Fire Detectors 
UQGS.S6228 - Heat-automatic Fire Detectors 
UROX.S6173 - Smoke-automatic Fire Detectors 
URRQ.S7452 - Smoke-automatic Fire Detector Accessories 
UTGT.S6173 Single- and Multiple-Station Smoke Alarms