WARNING! MANDATORY STOP USE.

December / 2021 - WARNING! MANDATORY STOP USE. Failure to do so may result in serious injury or death

 

At Honeywell, our mission is to be the global leader in personal protective equipment with innovative solutions that protect and save lives. In line with our commitment to our mission statement, we are writing to inform you that it has been determined through standard validation and testing processes that guarantee the safety of our products, that there is a flame risk associated with the affixed suspension loop labels on Revolution Arc Flash Harnesses with Suspension Loops (part series RKNARRL), as the materials used in those labels for the impacted models may ignite if exposed to an arc flash condition. While there have been NO reported incidents due to this nonconformity, continued use of the product for arc flash protection could result in serious injury or death..

Honeywell Personal Protective Equipment announces an immediate stop use of the Honeywell Miller Revolution RKNARRL series with suspension loops (impacted parts in the chart below) ONLY when used for arc flash protection.

The following documents provide detailed instructions on immediate actions you are required to take.

Identify if your material has been impacted by the recall with the below list and instructions.

Potentially impacted part numbers

170011/S/MBK
170011/UBK
170011/23XBK
RKNARRL-QC/S/MBK
RKNARRL-QC/UBK
RKNARRL-QC/XXL/XXXLB
RKNARRL-QC-BDP/S/MBK
RKNARRL-QC-BDP/UBK
RKNARRL-QC-BDP/XXL/X
RKNARRL-TB/S/MBK
RKNARRL-TB/UBK
RKNARRL-TB/3XBK
RNKARRL-TB-BDP/UBK
RKNARRL-TB-BDP/XXL/X

 

If you have products with part numbers from the potentially impacted part numbers list, complete the following steps:

1. Locate the label and review if the material was manufactured from June 30, 2020 and June 28, 2021

2. If your harness is on the potentially impacted part number list and is manufactured between June 30, 2020 and June 28, 2021, please request a replacement by completing the following:

If your harness is on the potentially impacted part number list and is manufactured between June 30, 2020 and June 28, 2021, please request a replacement by completing the following:

Product Information Documentation

Proof of Destruction

Click here and attach product information documentation and proof of destruction to submit your request.

Décembre 2021 – ATTENTION! ARRÊT D'UTILISATION OBLIGATOIRE. Le non-respect de cette consigne peut entraîner des blessures graves ou la mort.

 

Chez Honeywell, notre mission est d'être le leader mondial des équipements de protection individuelle avec des solutions innovantes qui protègent et sauvent des vies. Conformément à notre engagement envers notre énoncé de mission, nous vous écrivons pour vous informer qu'il a été déterminé par des processus de validation et de test standard qui garantissent la sécurité de nos produits, qu'il existe un risque de flamme associé aux étiquettes de boucle de suspension apposées sur Revolution. Harnais d'arc électrique avec boucles de suspension (pièces de la série RKNARRL), car les matériaux utilisés dans ces étiquettes pour les modèles impactés peuvent s'enflammer s'ils sont exposés à un arc électrique. Bien qu'aucun incident n'ait été signalé en raison de cette non-conformité, l'utilisation continue du produit pour la protection contre les arcs électriques pourrait entraîner des blessures graves ou la mort.

L'équipement de protection individuelle Honeywell annonce un arrêt immédiat de l'utilisation de la série Honeywell Miller Revolution RKNARRL avec boucles de suspension (pièces impactées dans le tableau ci-dessous) UNIQUEMENT lorsqu'elles sont utilisées pour la protection contre les arcs électriques.

Les documents suivants fournissent des instructions détaillées sur les mesures immédiates que vous devez prendre.

Identifiez si votre matériel a été touché par le rappel avec la liste et les instructions ci-dessous.

Numéros de pièces potentiellement impactés:

 

170011/S/MBK
170011/UBK
170011/23XBK
RKNARRL-QC/S/MBK
RKNARRL-QC/UBK
RKNARRL-QC/XXL/XXXLB
RKNARRL-QC-BDP/S/MBK
RKNARRL-QC-BDP/UBK
RKNARRL-QC-BDP/XXL/X
RKNARRL-TB/S/MBK
RKNARRL-TB/UBK
RKNARRL-TB/3XBK
RNKARRL-TB-BDP/UBK
RKNARRL-TB-BDP/XXL/X

 

Si vous avez des produits avec des numéros de référence de la liste des numéros de référence potentiellement concernés, procédez comme suit :

1. Localisez l'étiquette et vérifiez si le matériau a été fabriqué entre le 30 juin 2020 et le 28 juin 2021.

2. Si votre harnais figure sur la liste des numéros de pièce potentiellement concernés et est fabriqué entre le 30 juin 2020 et le 28 juin 2021, veuillez demander un remplacement en remplissant ce qui suit :

Si votre harnais figure sur la liste des numéros de pièce potentiellement concernés et est fabriqué entre le 30 juin 2020 et le 28 juin 2021, veuillez demander un remplacement en remplissant les éléments suivants:

Document d'information sur le produit

Instructions pour la preuve de destruction

Cliquez ici et joindre les documents requis pour soumettre votre demande.